AD40xx易于使用的功能
AD400x系列集成了易于使用的功能,可降低信号链功耗、降低信号链复杂性,并实现更高通道密度。高Z模式以及长采集阶段消除了对专用大功率高速ADC驱动器的需求。这扩展了低功耗精密放大器的范围,可以直接驱动这些ADC,同时仍然实现最佳性能。
AD40xx的输入范围压缩功能允许ADC驱动器放大器和ADC在共用电源轨上工作。输入范围压缩功能不需要负电源,并保留完整ADC代码范围。
低串行外设接口 (SPI) 时钟速率降低了数字输入/输出功耗,拓宽了处理器选项,并简化了数字隔离上发送数据的任务。
特性
- 吞吐量:最大2MSPS
- 易于使用的功能降低系统功耗和复杂性
- 输入过压钳位电路
- 减少非线性输入电荷反冲
- 高Z模式
- 长采集阶段
- 输入范围压缩
- 快速转换时间允许低SPI时钟速率
- SPI可编程模式、读/写功能、状态字
- 1.8V单电源供电,具有1.71V-5.5V逻辑接口
- SAR架构:无延迟/流水线延时
- 确保温度工作:−40°C至125°C
- 符合SPI/QSPI/MICROWIRE/DSP标准的串行接口
- 菊花链多个ADC和忙指示器的能力
- 10引脚封装: 3mm × 3mm LFCSP和3mm × 4.90mm MSOP
- AD4000/AD4004/AD4008具体特性
- INL:±1LSB(最大值)
- 确保16位无失码
- 低功耗
- 在2MSPS时为9.75mW,在1MSPS时为4.9mW,在500kSPS时为2.5mW(仅限VDD)
- 在10kSPS时为70μW,在2MSPS时为14mW(总计)
- 信噪比:在1kHz时为93dB(典型值),VREF=5V;在100kHz时为90dB(典型值)
- 总谐波失真:在1kHz时为−115dB(典型值),VREF=5V;在100kHz时为-95dB(典型值)
- 伪差分(单端)模拟输入范围:0V至VREF,其中VREF为2.4V至5.1V
- AD4002/AD4006/AD4010具体特性
- INL:±3.2LSB(最大值)
- 确保18位无失码
- 低功耗
- 在2MSPS时为9.75mW,在1MSPS时为4.9mW,在500kSPS时为2.5mW(仅限VDD)
- 在10kSPS时为70μW,在2MSPS时为14mW(总计)
- 信噪比:在1kHz时为95dB(典型值),VREF=5V;在100kHz时为95dB(典型值)
- 总谐波失真:在1kHz时为−125dB(典型值),VREF=5V;在100kHz时为-108dB(典型值)
- 伪差分(单端)模拟输入范围
- 0V至VREF,其中VREF为2.4V至5.1V
- 0V至VREF,其中VREF为2.4V至5.1V
- AD4003/AD4007/AD4011具体特性
- INL:最大值为±1LSB (±3.8ppm)
- 确保18位无失码
- 低功耗
- 在2MSPS时为9.5mW,在1MSPS时为4.9mW,在500kSPS时为2.4mW(仅限VDD)
- 在10kSPS时为80μW,在2MSPS时为16mW(总计)
- 信噪比:在1kHz时典型值为100.5dB,VREF=5V;在100kHz时典型值为99dB
- 总谐波失真:在1kHz时典型值为-123dB,VREF=5V;在100kHz时典型值为-100dB
- 差分模拟输入范围:±VREF
- 0V至VREF,其中VREF为2.4V至5.1V
应用
- 自动化测试设备
- 机械自动化
- 医疗设备
- 电池供电设备
- 精密数据采集系统
视频
评估板
EVAL-AD4000FMCZ 16位 2MSPS精密伪差分ADC评估板演示16位AD4000 ADC的性能,为各种系统应用提供易于理解的接口。
EVAL-AD4001FMCZ 16位2MSPS精密SAR差分ADC评估板演示16位AD4001和AD4005 ADC的性能。
EVAL-AD4002FMCZ 18位2 MSPS精密伪差分SAR ADC评估板演示AD4002、AD4006和AD4010模数转换器的性能。
EVAL-SDP-CH1Z 高速系统演示平台 包括一系列控制器板、插入器板和子板。SDP高速 (SDP-H1) 控制器板是EVAL-SDP-CH1Z SDP的一部分。设计人员可使用SDP-H1控制器板和评估板找出一种从评估中的系统与PC通信的方法。
Articles
Condition-Based Monitoring: The Wearable for Machine Health
Condition-based monitoring (CbM) is the Industry 4.0 equivalent of wearable fitness devices. With the explosion of connectivity comes the opportunity to observe the physical world like never before and to see physical processes in action, in real-time, in fine detail. Reduce unplanned downtime by understanding the aging process of equipment and machines.
How to Build a MEMS-Based Solution for Vibration Detection in Condition Monitoring
Condition monitoring is one of today’s core challenges in the use of mechanical facilities and technical systems to minimize the risk of production downtime not only in the industrial sector but wherever machines are used. In this article, a highly linear, low noise, wideband vibration measurement solution based on the ADXL1002 MEMS accelerometer is shown. This solution can be used for bearing analysis or engine monitoring and for all applications in which a large dynamic range of up to ±50g and a frequency response from DC to 11kHz are required.