SparkFun 工具与耗材

结果: 972
选择 图像 零件编号 制造商 描述 数据表 供货情况 单价(含13%增值税) 根据您的数量,按照单价筛选表格中的结果。 数量 RoHS
SparkFun SparkFun 配件 These are a pair of DG01D-E hobby motors with encoder with a hall speed encoder. The motor requires a voltage between 4.5-9V has a gearbox ratio of 1:48 and a speed of 140RPM at 4.5V. The voltage between positive and negative is determined according
SparkFun SparkFun 配件 This is not your normal Passive Infrared (PIR) sensor! The SparkFun AK9753 Human Presence Sensor Breakout is a Qwiic-enabled 4-channel Nondispersive Infrared (NDIR) sensor. Each channel has a different field of view so not only can the AK9753 detec

SparkFun SparkFun 配件 This is the main PCB assembly used in the RTK Facet and is intended for users who need to repair a device. Open Source Hardware has the benefit of allowing a user to understand and repair a broken device themselves! For more information please see t
SparkFun SparkFun 配件 This is the enclosure and various bits needed to replace the housing of an RTK Facet and is intended for users who need to repair a device. Open Source Hardware has the benefit of allowing a user to understand and repair a broken device themselves!
SparkFun SparkFun 配件 This is the enclosure and various bits needed to replace the housing of an RTK L-Band Facet. Open Source Hardware has the benefit of allowing a user to understand and repair a broken device themselves! For more information please see the disassembly
SparkFun SparkFun 配件 This is the main PCB assembly used in the RTK L-Band Facet and is intended for users who need to repair a device. Open Source Hardware has the benefit of allowing a user to understand and repair a broken device themselves! This board does not include
SparkFun SparkFun 配件 This is the black silicone protective sock that is stretched over the RTK Facet or RTK Facet L-Band and is intended for users who need to repair a device. Open Source Hardware has the benefit of allowing a user to understand and repair a broken devic
SparkFun SparkFun 配件 When you're working with e-textiles you have a tendency to collect a lot of small parts: LilyPad boards bobbins needles...the tools of the trade. Why not pick up a sturdy box to keep your bits and pieces off the floor? This large LilyPad-branded b

SparkFun SparkFun 配件 These coated flat endmills are perfect for cutting aluminum. They have a ZrN coating which provides a better finish longer lifespan and a superior cut compared to a non-coated endmill.This cutter has a shorter flute length to provide greater rigidi
SparkFun SparkFun 配件 These flat mills are perfect for roughing or machining flat or prismatic parts.If you've got a Nomad or Shapeoko these are great cutters for cutting plastic and aluminum.All of our cutters are manufactured here in the US and begin life as a blank of
SparkFun SparkFun 配件 These flat mills are perfect for roughing or machining flat or prismatic parts.If you've got a Nomad or Shapeoko these are great cutters for cutting plastic and aluminum.All of the cutters are manufactured here in the US and begin life as a blank of
SparkFun SparkFun 配件 These flat mills are perfect for roughing or machining flat or prismatic parts.If you've got a Nomad or Shapeoko these are great cutters for cutting plastic and aluminum.All of the cutters are manufactured here in the US and begin life as a blank of
SparkFun SparkFun 配件 Just bought your machine and not sure what endmills you should get? The Shapeoko Endmill Starter Pack is for you! It contains a variety of the most popular endmills used on the Shapeoko to get you going on a variety of projects.
SparkFun SparkFun 配件 USB as a power connection standard is common these days but you don't always have a computer on hand so how are you going to power all of your sweet USB devices? How about a high quality switching 'wall wart'? This AC to DC power supply will do 5V a

SparkFun SparkFun 配件 Please note these machines are built to order & have an estimated lead time of 10 days before shipping This is the Shapeoko Standard Z-Plus No Router 65mm a desktop 3-axis CNC Machine kit that allows you to create your 2D and 3D designs out of non
SparkFun SparkFun 配件 Please note these machines are built to order & have an estimated lead time of 10 days before shipping This is the Shapeoko Standard Z-Plus No Router 65mm a desktop 3-axis CNC Machine kit that allows you to create your 2D and 3D designs out of non
SparkFun SparkFun 配件 Please note these machines are built to order & have an estimated lead time of 10 days before shipping This is the Shapeoko XL nearly double the cutting area of the Shapeoko Standard! The Shapeoko is a 3-axis CNC Machine kit that allows you to crea
SparkFun SparkFun 配件 Please note these machines are built to order & have an estimated lead time of 10 days before shipping This is the Shapeoko XL nearly double the cutting area of the Shapeoko Standard! The Shapeoko is a 3-axis CNC Machine kit that allows you to crea
SparkFun SparkFun 配件 Please note these machines are built to order & have an estimated lead time of 10 days before shipping This is the Shapeoko XXL nearly FOUR times the cutting area of the Shapeoko Standard! That s a lot of cutting area! The Shapeoko is a 3-axis CN
SparkFun SparkFun 配件 Please note these machines are built to order & have an estimated lead time of 10 days before shipping This is the Shapeoko XXL nearly FOUR times the cutting area of the Shapeoko Standard! That s a lot of cutting area! The Shapeoko is a 3-axis CN
SparkFun SparkFun 配件 This is a PCB edge mount SMA RF connector. These connectors are perfect for prototyping with the GPS and Cellular devices that require an antenna connection. Each connector is equipped with a female signal pin and will correctly mate with the origin
SparkFun 书籍及媒体 The full-color SparkFun Inventor's Kit Guidebook V3 contains step by step instructions of how to connect each circuit with the included parts. Full example code is provided and explained and even includes troubleshooting tips if something goes wrong.
SparkFun SparkFun 配件 RGB LED Matrix Panel - 32x32
SparkFun SparkFun 配件 The Bourns Absolute Encoder is a digital control knob that provides 128 unique results evenly spaced around a full circle. It is designed as a control panel knob but can be adapted for other uses. This can be a good alternative to using a potentiomet
SparkFun SparkFun 配件 This SparkFun Qwiic Pro Micro BoogieBoard was a limited edition version of the Qwiic Pro Micro. We are now out of stock and are not reproducing it. The SparkFun Qwiic Pro Micro BoogieBoard is a Special Edition version of the SparkFun Qwiic Pro Micro