Freescale S12ZVC MagniV Mixed-Signal MCU from Mouser Supports MSCAN, SENT, and LIN
May 6, 2015 - Mouser Electronics, Inc., the global authorized distributor with the newest semiconductors and electronic components, is now stocking the new S12ZVC MagniV™ Mixed-Signal Microcontroller from Freescale Semiconductor. The Freescale® S12ZVC 16‑bit microcontroller is based on a 32 MHz S12Z core and has 192 KBytes of Flash memory, 12 KBytes of RAM, 2 KBytes of EPROM, integrates CAN Physical Layer, a 12‑bit analog to digital converter (ADC), 8‑bit DAC, and more. The S12ZVC supports a number of automotive and industrial communications protocols, including SENT, MSCAN, and LIN.
The new Freescale S12ZVC MagniV Mixed-Signal Microcontroller, available from Mouser Electronics, is a highly integrated mixed-signal microcontroller that includes a 12 V voltage regulator, analog peripherals, and automotive/industrial serial protocols on a single chip. The S12ZVC is based on a high performance 16‑bit core that includes a 32‑bit ALU and a 24‑bit address space. Integrated CAN physical layer with high immunity to EMI and 8 kV ESD resistance provides reliable operation in harsh environments. Sixteen channels of 12‑bit ADC and a single 8‑bit 5 V digital-to-analog converter (DAC) provide analog signal capture and generation. Four pins support 25 mA sink and one pin supports 20 mA source currents for driving high current loads. The S12ZVC is capable of operating at high ambient temperature of up to 150°C, making it an ideal solution for space constrained and high temperature applications.
The S12ZVC supports a number of automotive and industrial communications interfaces. The robust SAE J2716 SENT (Single Edge Nibble Transmission) serial data protocol is for communicating with sensors in harsh environments. The MSCAN serial interface is based on the CAN 2.0B protocol and uses an advanced buffer arrangement system that results in predictable real-time behavior, making the protocol suitable for automotive, industrial, and general embedded applications. Two SCI interfaces support the LIN serial protocol.
Target applications for the Freescale S12ZVC include automotive applications, CAN-based sensors, HVAC controllers, lighting control, and industrial applications.
To learn more, visit: http://www.mouser.com/new/Freescale-Semiconductor/freescale-s12zvc-mcu/ .
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser Electronics
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com